DOUT.STATES
Description
DOUT.STATES reads the states of the digital outputs. Each bit corresponds to a digital state. Bit 0 = DOUT1 ... Bit 8 = DOUT9.
Examples
Usage
When DOUT1 and DOUT3 are active (DOUT#.STATE = 1). Bits 0 and 2 would be set. DOUT.STATES would be 5.
Code
--> DOUT.STATES 5
Context
See Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 511 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DOUT.STATES |
3600h |
00h |
Unsigned32 |
- |
- |
Read only |
Yes |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2702 |
1 |
2702 (0xa8e) |
DOUT.STATES |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DOUT.STATES |
2702 |
Unsigned32 |
Read Only |
- |